This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Two PUMPREQUEST Registers?

Part Number: TMS320F28388D

Greetings,

I had noticed that the PUMPREQUEST register had moved between the 379 and the 388 and is now in the IPC registers as can be seen in spruii0e Table 16-7.  But it also exists in Table 13-67.  The two definitions are the same.  There is an address for it from the IPC registers, but none from the Flash Registers section.  Is the information in Table 13-67 supposed to be there?  Or is there a second way to get to that register?

Thank you,

Ed