Part Number: TMS320F28379D
Due to most of the processor pins being used, my company chose not to connect the EM1A11 and EM1A10 pins to the SDRAM, thinking that this would only sacrifice some addresses (the processor is using these pins for the SPI interface). But now, reading the documentation, I realize that the EM1A10 pin has a specific functionality related to the PRE command. Is it possible to communicate with SDRAM memory without using these pins? And what would the configuration of the EMIF registers be like in this case?
SDRAM being used: AS4C8M32S-6TIN 256Mbits x 16 bits x 4 banks