This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Communications types recommended for collecting data from MSP430's and processing on C2000

Looking at different ways of transmitting very small amounts of data between MSP430's and C2000 and hoping to get some real world input.

 

Distance between devices is up to 150 feet.

Wired and possible wireless (thoughts on ZigBee?)

Multiple (less than 25) MSP430's to one C2000

C2000 has separate constant USB or TCP/IP

 

Thoughts on protocols and physical paths is appreciated.