Part Number: TMS320F28335
Other Parts Discussed in Thread: UNIFLASH, C2000WARE
I am using CCS 8.3.1 and an XDS110 with a custom board. I have read a lot of good information about the code security module but I am really not sure procedurally how to use it there must be a description somewhere. What are the steps?
I have my production code ready and want to be able to lock the part before shipping the hardware but i want to try it out:
- How do i set the password - if the answer is ccs i dont see the "on-chip flash" option under tools
- I want to verify it is locked
- I want to try getting back into it in case i need to make a change
- can i set the password back to all 1 to get back to development if needed
- what code do i need in my application? i have CsmUnlock() from the example not sure it is run though, do i need it or is the key read as part of bootloader?
Any help would be appreciated. Thanks!