This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: Using the xintf_run_from routine, an exception occurs after running and the program stops

Part Number: TMS320F28335

Is there a problem with the external ram or wiring?

Example_2833xCodeRunFromXintf [Code Composer Studio - Device Debugging]
Texas Instruments XDS2xx USB Debug Probe/C28xx (Suspended - SW Breakpoint)
ILLEGAL_ISR() at DSP2833x_DefaultIsr.c:185 0x00906E
_args_main() at args_main.c:137 0x00975F
cpu_timer0_isr() at Example_2833xCodeRunFromXintf.c:236 0x200001
_system_post_cinit() 0x1F3000 (an error occurred: failed to parse the previous frame FP)

--

Thanks & Regards