This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Maximum CLK speed for McBSP module in the F28335

Hello,

 

I am trying to configure the McBSP module in the F28335. I want to connect it to an external clock via MCLKR pin. What is the maximum clock rate (CPU speed is 150MHz) possible?? Is 20MHz ok?

 

Thanks!

Dror