Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: C2000WARE
Hello,
Is there any example of using Secure ROM Function APIs with F28P65x? I want to use CMAC Calculation Function in my bootloader
I couldn't find any example for F28P65x, so I took example code from F2838x, put it in a F28P65x project. The build fails at the linker:
error #16004-D: file "C:/ti/c2000/C2000Ware_5_01_00_00/libraries/boot_rom/f28P65x/rev0/rom_symbol_libs/cpu1/SafeZoneCode/lib/f28P65xCPU1_SecureZoneCodeSymbols_fpu32.lib<F28006x_CPU1_ROM_out_CPU1BROM_calculateCMAC_tmp.obj>" has a Tag_VCU attribute value of "1" that is different than one previously seen ("3"); combining incompatible files
Any idea?
CCS Version: 12.5.0.00007
C2000Ware Version: 5.01.0.0
Thanks,
Kinjeo