Part Number: TMS320F280039C
Hello Ti,
I am trying to read the offset of the AD module, but I am having issues with it.
VREFLO (internal connection). Do I have to enable anything else besides mapping the AD signal, in this case A or B or C 13 to the ADCSOC that I want to use?
I have my analog reference module configured to external reference and the reference mode of 1.65V.
I am currently reading a value of only 8IU (12bit value) and I am not sure if that would be accurate.
Also, do I have to perform the conversions for each module (Adca, Adcb, Adcc) and set the corresponding OFFTRIMS for each module?
The reference that I used is a 28006x which had a slightly different approach to this method:
I would like to use this offset in other computations, so I'd like to avoid last step from 39C.
Any info and help is much appreciated, thank you.