Part Number: TMS320F28377S
Hello,
I am using eCAP to get the duty cycle of input PWM signal. (50Hz)
However in my Motor Control Application there is some switching noise that probably corrupts eCAP reading.
What I see on a scope is some nano-second gliches of amplitude 1V, sometimes 2V, but not sure if this are what really is on the uC pin or this is induced in scope probe (so false measurement)
Nontheless I am getting wrong readings from eCAP when start switching (3-phase inverter).
Is there a way to cope with this on the software/eCAP configuration level?
I will try in a mean time add some filtering on PCB but I would prefer to fix it in SW.
As my signal i want to measure is low freq and those gliches are of ns or sub-ns duration.
Regards,
Adam