Other Parts Discussed in Thread: DAC70501
Hi everyone,
I having problems to configure the SPI 3-wire mode, to simply send 3 bytes to an SPI slave.
The GPIOs are correctly configured:
SysCtrlRegs.PCLKCR0.bit.SPIAENCLK = 1; // SPI-A //-------------------------------------------------------------------------------------- // GPIO-16 - PIN FUNCTION = SPISIMO-A GpioCtrlRegs.GPAPUD.bit.GPIO16 = 0; // Enable pull-up on GPIO16 (SPISIMOA) GpioCtrlRegs.GPAQSEL2.bit.GPIO16 = 3; // Asynch input GPIO16 (SPISIMOA) GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 1; // 0=GPIO, 1=SPISIMO-A, 2=Resv, 3=TZ2 //-------------------------------------------------------------------------------------- // GPIO-17 - PIN FUNCTION = SPISOMI-A (as GPIO not needed in 3-wire mode) GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 0; // 0=GPIO, 1=SPISOMI-A, 2=Resv, 3=TZ3 GpioCtrlRegs.GPADIR.bit.GPIO17 = 1; // 1=OUTput, 0=INput GpioDataRegs.GPACLEAR.bit.GPIO17 = 1; // uncomment if --> Set Low initially //-------------------------------------------------------------------------------------- // GPIO-18 - PIN FUNCTION = SPICLK-A GpioCtrlRegs.GPAPUD.bit.GPIO18 = 0; // Enable pull-up on GPIO18 (SPICLKA) GpioCtrlRegs.GPAQSEL2.bit.GPIO18 = 3; // Asynch input GPIO18 (SPICLKA) GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 1; // 0=GPIO, 1=SPICLK-A, 2=SCITX-A, 3=XCLKOUT //-------------------------------------------------------------------------------------- // GPIO-19 - PIN FUNCTION = SPISTE-A GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0; // Enable pull-up on GPIO19 (SPISTEA) GpioCtrlRegs.GPAQSEL2.bit.GPIO19 = 3; // Asynch input GPIO19 (SPISTEA) GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 1; // 0=GPIO, 1=SPISTE-A, 2=SCIRX-A, 3=ECAP1 //--------------------------------------------------------------------------------------
Then I initialised the FIFO with 3 levels for TX, I do not need RX (or maybe yes?):
void spi_fifo_init()
{
// Initialize SPI FIFO registers
//SpiaRegs.SPIFFTX.all=0xE040;
SpiaRegs.SPIFFTX.bit.SPIRST=1; //SPI FIFO can resume transmit or receive
SpiaRegs.SPIFFTX.bit.SPIFFENA=1; //SPI FIFO enhancements are enabled
SpiaRegs.SPIFFTX.bit.TXFFINTCLR =1; // Clear TXFIFO interrupt flag
SpiaRegs.SPIFFTX.bit.TXFFIENA = 0; // TXFIFO interrupt disabled
SpiaRegs.SPIFFTX.bit.TXFFIL =3; //3 levels for TXFIFO Interrupt (no needed)
SpiaRegs.SPIFFTX.bit.TXFIFO =1; //Release transmit FIFO from reset.
//SpiaRegs.SPIFFRX.all=0x2044;
SpiaRegs.SPIFFRX.bit.RXFFOVFCLR = 1; // CLEAR OV rX flag
SpiaRegs.SPIFFRX.bit.RXFFINTCLR =1; //b6 Clear SPIFFRX flag
SpiaRegs.SPIFFRX.bit.RXFFIENA = 0; //b5 RXFIFO interrupt disabled
SpiaRegs.SPIFFRX.bit.RXFFIL=0; //level bits for RXFIFO Interrupt (no needed)
SpiaRegs.SPIFFRX.bit.RXFIFORESET = 1; //b13 Re-enable receive FIFO operation.
SpiaRegs.SPIFFCT.all=0x0; //The next word in the TX FIFO buffer is transferred to
//SPITXBUF immediately upon completion of transmission of the
//previous word.
}
Then SPI initialisation :
void spi_init_DAC70501()
{
//SpiaRegs.SPICCR.all =0x000F; // Reset on, rising edge, 16-bit char bits
//SpiaRegs.SPICTL.all =0x0006; // Enable master mode, normal phase,
// enable talk, and SPI int disabled.
SpiaRegs.SPICCR.bit.SPISWRESET = 0; //Reset SPI before configuration
SpiaRegs.SPICCR.bit.CLKPOLARITY =1; //falling edge
SpiaRegs.SPICCR.bit.SPICHAR =7; //8-bit char bits
SpiaRegs.SPICTL.bit.MASTER_SLAVE=1; //Enable master mode
SpiaRegs.SPICTL.bit.CLK_PHASE=1; // phase with delay
SpiaRegs.SPICTL.bit.TALK = 1; // Enable Transmit path
SpiaRegs.SPICTL.bit.OVERRUNINTENA = 0; //disbale overrun interruption
SpiaRegs.SPICTL.bit.SPIINTENA = 0; ////disable SPIinterruption
SpiaRegs.SPIBRR =127; // SPI Baud Rate=LSPCLK/(SPIBRR+1) LSPCLK=CPU_FREQ/4
// 15MHz/(127+1)=117kHz
// 15MHz/(14+1)=1MHz
SpiaRegs.SPIPRI.bit.TRIWIRE=1; //3-wire SPI mode enable
//(The unused pin SPISOMI is free for GPIO)
//SpiaRegs.SPICCR.all =0x009F; // Relinquish SPI from Reset
SpiaRegs.SPICCR.bit.SPISWRESET = 1; // Relinquish SPI from Reset
SpiaRegs.SPIPRI.bit.FREE = 1; // Set so breakpoints don't disturb xmission
}
And finally this is the TX function I am periodically calling in the main program:
/**********************************************************************
* Function: spi_xmit()
*
* Description: Transmit 16bit to SPIA using 3-Wire Mode Transmit
* When the master transmits, it receives the data it
* transmits (because SPISIMOx and SPISOMIx are connected
* internally in 3-wire mode). Therefore, the junk data received
* must be cleared from the receive buffer every time data is transmitted.
**********************************************************************/
void spi_xmit(char a)
{
Uint16 data= (Uint16)(a<<8);
Uint16 dummy;
SpiaRegs.SPICTL.bit.TALK = 1; // Enable Transmit path
SpiaRegs.SPITXBUF = data; // Master transmits data
while(SpiaRegs.SPISTS.bit.INT_FLAG !=1) {} // Waits until data rx’d
dummy = SpiaRegs.SPIRXBUF; // Clears junk data from itself
SpiaRegs.SPITXBUF = data; // Master transmits data
while(SpiaRegs.SPISTS.bit.INT_FLAG !=1) {} // Waits until data rx’d
dummy = SpiaRegs.SPIRXBUF; // Clears junk data from itself
SpiaRegs.SPITXBUF = data; // Master transmits data
while(SpiaRegs.SPISTS.bit.INT_FLAG !=1) {} // Waits until data rx’d
dummy = SpiaRegs.SPIRXBUF; // Clears junk data from itself
}
I can check in the oscilloscope that the 1st byte is sent but the communication gets block after that.
Without 3-wire mode or FIFO, I am able to send 2bytes without problems (no blocking).
What I am doing wrong? What is the right way to simply send 3 bytes by SPI to an external slave ?
Thanks in advance.
Best regards