Part Number: TMS320F28377D
Hello:
Regarding the customer's power filter project, if there are any issues, please help to take a look; Thank you!
The client has been using version 6.1.0 of the compiler, but now they need to use 28377 with CLA suffix, which is causing a compilation error;
1. When the customer is using your DSP, only version 6.1.0 of the compiler can be used normally, and other compilers are not working;
2. If CLA is not used, it is possible to compile 28377 in version 6.1.0. However, compiling 28377 with CLA at the tail may cause compilation issues
3. Except for version 6.1.0, all other versions can compile 28377 with CLA, but there are some waveform issues;
4. The 28335 and 28346 programs are the same, that is, if you change the compiler, the 6.1.0 waveform is OK, but if you change it to another compiler waveform, there is a problem;