Other Parts Discussed in Thread: TMDSDOCK28379D
We are currently working with the following TI components:
- TMDSDOCK28379D dev hardware.
- C2000 Ware 5.00
- CSS 12.40
The board clocks are configured as follows:
- CPU1.SYSCLK = 200MHz
In the TMS320F2837xS Reference Manual (SPRUHX5G–August 2014–Revised September 2019) para 23.4.9 & table 23-2 describes the access to the message RAMs from the DMA & CPU/CLA views. Based on the address ranges specified, it seems that the address ranges have been swapped (typo).
Can someone confirm this?