Part Number: TMS320F28386D
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Hello.
I would like to ask you a question about how to convert data input in parallel into series.

The figure above is the data output waveform of AFE5401(TI ADC).
As shown in the figure, signals are being output in parallel from D0 to D11 pins.
And I would like to show it as a serial signal like CH1 ~ CH4.
The SYSCLK of tms320f28386d is 200 MHz, and the DCLK output from ADC (AFE5401) is 1.5625 MHz.
Ultimately, what I want to know is whether it can be implemented as a program without an external shift register.
Is it possible to implement it with GPIO? If you tell me various ways to implement it, I will try it. I would appreciate it if you could also suggest an example.
I desperately hope that I can get help.
Thank you.