This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28384D: How can i add sysconfig GUI to a project i am coding for this chip

Part Number: TMS320F28384D
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE

Hello. 

I recently embedded my own TMS320F28384D chip making a custom testboard for myself. I am able to get the board up and running perfectly with the XDS110 jtag prob, i can flash code to RAM and to ROM on the chip and i tested this by making a simple LED blink program. 

HOWEVER, since this is not a luanchpad or a control card, i cannot find an example empty project for the chip i am using that already has sysconfig working on the project. So i tried to add it by adding a new file to the project and naming it "test_project.syscfg. This successfully pulled up a sysconig file, and i was prompted to add it to the project linker which I clicked "yes" to do.

Then, i selected the correct package and pin package and all and then hit save. Now, when i try and build the project it won't build anymore. Instead I get this error:

subdir_rules.mk:23: recipe for target 'build-1632660079' failed
Missing argument: --board or --device must be specified
gmake: *** [build-1632660079] Error 1
gmake: Target 'all' not remade because of errors.

Also when i click out of sysconfig in the project and then click back into it, i get this error: 

please help me know what is happening here. thanks.