Other Parts Discussed in Thread: UNIFLASH
Hi,
I am using the F28379D Control card for my project with Code Composer Studio12.1IDE and debug probe is xds100v2 . I want to load the code (i.e .out file) using the Uniflash 8.0 provided by TI. I have the JTAG Interface for code loading .
1 . While trying to detect the target device in uniflash , I am not able to detect the device it is continuously showing loading....... I try to detect for 5 mins also but still no success.
2. After that try to detect the device manually also , I have selected the f28379d Launchpad and debug probe as xds100v2 in the Uniflash given menu and try to erase the flash but for that also it is showing loading......... As shown below.
Could you please suggest what Can be problem?
Warm Regards
Annu