Part Number: TMS320F280025C
I get the error Error -267 @ 0x0 when I trying to program a TMSF280025C on a custom board through a blackhawk isolator and XDS110 probe.

However, I do not get the error when I use the 'test connection' option for the target configuration file to test the connection. The test is passed successfully.

I have verified that there is no issue with either the target configuration file or the custom board since I can program it successfully if I use the same files using a different laptop. This issue only occurs when I use a specific laptop. However, as I mentioned, the connection test is passed on this same laptop. Any tips on how to debug this or what the possible cause for this would be most welcome. Shown below are my target config settings.