Part Number: TMS320F28375S
Other Parts Discussed in Thread: SYSCONFIG, , C2000WARE
Hello guys,
my code is based on TMS320F28375S and i am debugging it in Launchpad 28379D. I have configured I2C by sysconfig tool as shown in image below.

I have knowledge about I2C protocol but i don't know how it is working in ccs (TI controllers)
this is a part of my code which is used for I2C
void main()
{
myI2C0_init();
//-----------------------------------//
// while loop from main()
while(1)
{
while(I2C_isBusBusy(myI2C0_BASE)); // bus check
I2C_sendStartCondition(myI2C0_BASE); // start
I2C_putData(myI2C0_BASE, 0xB4); // addr + 0 (write)
I2C_putData(myI2C0_BASE, 0x20); // read reg no 32
I2C_sendStartCondition(myI2C0_BASE); // repeated start
I2C_putData(myI2C0_BASE, 0xB5); // addr + 1 (read)
I2C_buf[0] = I2C_getData(myI2C0_BASE); // read MSB
I2C_sendNACK(myI2C0_BASE); // send NACK
I2C_buf[1] = I2C_getData(myI2C0_BASE); // read LSB
I2C_sendNACK(myI2C0_BASE); // send NACK
I2C_sendStopCondition(myI2C0_BASE); // stop
while (I2C_getStopConditionStatus(myI2C0_BASE)); // stop status
}
}
// I2C init function in Board.c file //
void myI2C0_init(){
I2C_disableModule(myI2C0_BASE);
I2C_initController(myI2C0_BASE, DEVICE_SYSCLK_FREQ, 400000, I2C_DUTYCYCLE_33);
I2C_setConfig(myI2C0_BASE, I2C_CONTROLLER_SEND_MODE);
I2C_setTargetAddress(myI2C0_BASE, 90);
I2C_disableLoopback(myI2C0_BASE);
I2C_setBitCount(myI2C0_BASE, I2C_BITCOUNT_8);
I2C_setDataCount(myI2C0_BASE, 2);
I2C_setAddressMode(myI2C0_BASE, I2C_ADDR_MODE_7BITS);
I2C_disableFIFO(myI2C0_BASE);
I2C_setEmulationMode(myI2C0_BASE, I2C_EMULATION_STOP_SCL_LOW);
I2C_enableModule(myI2C0_BASE);
}
my slave address is 90(decimal).
the I2C is not working as per this. sometimes the bus is busy and sometimes i get stucked while getting stop conditon status.
please help me to get data from AM4096.
thanks in advance.
regards
Muzammil Qureshi