Part Number: TMDSCNCD28388D
Other Parts Discussed in Thread: SYSCONFIG
Hello,
related from my help request of this thread: e2e.ti.com/.../tms320f28386d-i2c-communication-problem-i2c_ex2_eeprom-ti-example
Now I have the TMDSCNCD28388D board available to do this type of test, I'm back to try "i2c_ex2_eeprom" basic (with the I2CA) and the result is the read operation always returns 0xFF (255).

I setted the Target address to 0x51 because from the datasheet of Eeprom (24LC512) and from my electrical scheme: 1010(control code) + 0(a2) + 0(a1) +1(a0)
I configured with Sysconfig the WP pin: Output(push-pull) and Initial value 0 low (to disable the write protection).

//#############################################################################
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
//
// Defines
//
#define TARGET_ADDRESS 0x51
#define EEPROM_HIGH_ADDR 0x00
#define EEPROM_LOW_ADDR 0x30
#define NUM_BYTES 8
#define MAX_BUFFER_SIZE 14 // Max is currently 14 because of
// 2 address bytes and the 16-byte
// FIFO
//
// I2C message states for I2CMsg struct
//
#define MSG_STATUS_INACTIVE 0x0000 // Message not in use, do not send
#define MSG_STATUS_SEND_WITHSTOP 0x0010 // Send message with stop bit
#define MSG_STATUS_WRITE_BUSY 0x0011 // Message sent, wait for stop
#define MSG_STATUS_SEND_NOSTOP 0x0020 // Send message without stop bit
#define MSG_STATUS_SEND_NOSTOP_BUSY 0x0021 // Message sent, wait for ARDY
#define MSG_STATUS_RESTART 0x0022 // Ready to become controller-receiver
#define MSG_STATUS_READ_BUSY 0x0023 // Wait for stop before reading data
//
// Error messages for read and write functions
//
#define ERROR_BUS_BUSY 0x1000
#define ERROR_STOP_NOT_READY 0x5555
#define SUCCESS 0x0000
//
// Typedefs
//
struct I2CMsg {
uint16_t msgStatus; // Word stating what state msg is in.
// See MSG_STATUS_* defines above.
uint16_t TargetAddr; // Target address tied to the message.
uint16_t numBytes; // Number of valid bytes in message.
uint16_t memoryHighAddr; // EEPROM address of data associated
// with message (high byte).
uint16_t memoryLowAddr; // EEPROM address of data associated
// with message (low byte).
uint16_t msgBuffer[MAX_BUFFER_SIZE]; // Array holding message data.
};
//
// Globals
//
struct I2CMsg i2cMsgOut = {MSG_STATUS_SEND_WITHSTOP,
TARGET_ADDRESS,
NUM_BYTES,
EEPROM_HIGH_ADDR,
EEPROM_LOW_ADDR,
0x01, // Message bytes
0x23,
0x45,
0x67,
0x89,
0xAB,
0xCD,
0xEF};
struct I2CMsg i2cMsgIn = {MSG_STATUS_SEND_NOSTOP,
TARGET_ADDRESS,
NUM_BYTES,
EEPROM_HIGH_ADDR,
EEPROM_LOW_ADDR};
struct I2CMsg *currentMsgPtr; // Used in interrupt
uint16_t passCount = 0;
uint16_t failCount = 0;
//
// Function Prototypes
//
void initI2C(void);
uint16_t readData(struct I2CMsg *msg);
uint16_t writeData(struct I2CMsg *msg);
void fail(void);
void pass(void);
__interrupt void i2cAISR(void);
//
// Main
//
void main(void)
{
uint16_t error;
uint16_t i;
//
// Initialize device clock and peripherals
//
Device_init();
//
// Disable pin locks and enable internal pullups.
//
Device_initGPIO();
//
// Initialize GPIOs for use as SDA A and SCL A respectively
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_SDAA);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SDAA, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SDAA, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(DEVICE_GPIO_CFG_SCLA);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SCLA, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCLA, GPIO_QUAL_ASYNC);
//
// Initialize PIE and clear PIE registers. Disable CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// Interrupts that are used in this example are re-mapped to ISR functions
// found within this file.
//
Interrupt_register(INT_I2CA, &i2cAISR);
//
// Set I2C use, initializing it for FIFO mode
//
initI2C();
//
// Clear incoming message buffer
//
for (i = 0; i < MAX_BUFFER_SIZE; i++)
{
i2cMsgIn.msgBuffer[i] = 0x0000;
}
//
// Set message pointer used in interrupt to point to outgoing message
currentMsgPtr = &i2cMsgOut;
//
// Enable interrupts required for this example
//
Interrupt_enable(INT_I2CA);
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//
EINT;
ERTM;
//
// Loop indefinitely
//
while(1)
{
//
// **** Write data to EEPROM section ****
//
// Check the outgoing message to see if it should be sent. In this
// example it is initialized to send with a stop bit.
//
if(i2cMsgOut.msgStatus == MSG_STATUS_SEND_WITHSTOP)
{
//
// Send the data to the EEPROM
//
error = writeData(&i2cMsgOut);
//
// If communication is correctly initiated, set msg status to busy
// and update currentMsgPtr for the interrupt service routine.
// Otherwise, do nothing and try again next loop. Once message is
// initiated, the I2C interrupts will handle the rest. See the
// function i2cAISR().
//
if(error == SUCCESS)
{
currentMsgPtr = &i2cMsgOut;
i2cMsgOut.msgStatus = MSG_STATUS_WRITE_BUSY;
}
}
//
// **** Read data from EEPROM section ****
//
// Check outgoing message status. Bypass read section if status is
// not inactive.
//
if (i2cMsgOut.msgStatus == MSG_STATUS_INACTIVE)
{
//
// Check incoming message status
//
if(i2cMsgIn.msgStatus == MSG_STATUS_SEND_NOSTOP)
{
//
// Send EEPROM address setup
//
while(readData(&i2cMsgIn) != SUCCESS)
{
//
// Maybe setup an attempt counter to break an infinite
// while loop. The EEPROM will send back a NACK while it is
// performing a write operation. Even though the write
// is complete at this point, the EEPROM could still be
// busy programming the data. Therefore, multiple
// attempts are necessary.
//
}
//
// Update current message pointer and message status
//
currentMsgPtr = &i2cMsgIn;
i2cMsgIn.msgStatus = MSG_STATUS_SEND_NOSTOP_BUSY;
}
//
// Once message has progressed past setting up the internal address
// of the EEPROM, send a restart to read the data bytes from the
// EEPROM. Complete the communique with a stop bit. msgStatus is
// updated in the interrupt service routine.
//
else if(i2cMsgIn.msgStatus == MSG_STATUS_RESTART)
{
//
// Read data portion
//
while(readData(&i2cMsgIn) != SUCCESS)
{
//
// Maybe setup an attempt counter to break an infinite
// while loop.
//
}
//
// Update current message pointer and message status
//
currentMsgPtr = &i2cMsgIn;
i2cMsgIn.msgStatus = MSG_STATUS_READ_BUSY;
}
}
}
}
//
// Function to configure I2C A in FIFO mode.
//
void initI2C()
{
//
// Must put I2C into reset before configuring it
//
I2C_disableModule(I2CA_BASE);
//
// I2C configuration. Use a 400kHz I2CCLK with a 33% duty cycle.
//
I2C_initController(I2CA_BASE, DEVICE_SYSCLK_FREQ, 400000, I2C_DUTYCYCLE_33);
I2C_setBitCount(I2CA_BASE, I2C_BITCOUNT_8);
I2C_setTargetAddress(I2CA_BASE, TARGET_ADDRESS);
I2C_setEmulationMode(I2CA_BASE, I2C_EMULATION_FREE_RUN);
//
// Enable stop condition and register-access-ready interrupts
I2C_enableInterrupt(I2CA_BASE, I2C_INT_STOP_CONDITION |
I2C_INT_REG_ACCESS_RDY);
//
// FIFO configuration
//
I2C_enableFIFO(I2CA_BASE);
I2C_clearInterruptStatus(I2CA_BASE, I2C_INT_RXFF | I2C_INT_TXFF);
//
// Configuration complete. Enable the module.
//
I2C_enableModule(I2CA_BASE);
}
//
// Function to send the data that is to be written to the EEPROM
//
uint16_t writeData(struct I2CMsg *msg)
{
uint16_t i;
//
// Wait until the STP bit is cleared from any previous controller
// communication. Clearing of this bit by the module is delayed until after
// the SCD bit is set. If this bit is not checked prior to initiating a new
// message, the I2C could get confused.
//
if(I2C_getStopConditionStatus(I2CA_BASE))
{
return(ERROR_STOP_NOT_READY);
}
//
// Setup target address
//
I2C_setTargetAddress(I2CA_BASE, TARGET_ADDRESS);
//
// Check if bus busy
//
if(I2C_isBusBusy(I2CA_BASE))
{
return(ERROR_BUS_BUSY);
}
//
// Setup number of bytes to send msgBuffer and address
//
I2C_setDataCount(I2CA_BASE, (msg->numBytes + 2));
//
// Setup data to send
//
I2C_putData(I2CA_BASE, msg->memoryHighAddr);
I2C_putData(I2CA_BASE, msg->memoryLowAddr);
for (i = 0; i < msg->numBytes; i++)
{
I2C_putData(I2CA_BASE, msg->msgBuffer[i]);
}
//
// Send start as controller transmitter
//
I2C_setConfig(I2CA_BASE, I2C_CONTROLLER_SEND_MODE);
I2C_sendStartCondition(I2CA_BASE);
I2C_sendStopCondition(I2CA_BASE);
return(SUCCESS);
}
//
// Function to prepare for the data that is to be read from the EEPROM
//
uint16_t readData(struct I2CMsg *msg)
{
//
// Wait until the STP bit is cleared from any previous controller
// communication. Clearing of this bit by the module is delayed until after
// the SCD bit is set. If this bit is not checked prior to initiating a new
// message, the I2C could get confused.
//
if(I2C_getStopConditionStatus(I2CA_BASE))
{
return(ERROR_STOP_NOT_READY);
}
//
// Setup target address
//
I2C_setTargetAddress(I2CA_BASE, TARGET_ADDRESS);
//
// If we are in the the address setup phase, send the address without a
// stop condition.
//
if(msg->msgStatus == MSG_STATUS_SEND_NOSTOP)
{
//
// Check if bus busy
//
if(I2C_isBusBusy(I2CA_BASE))
{
return(ERROR_BUS_BUSY);
}
//
// Send data to setup EEPROM address
//
I2C_setDataCount(I2CA_BASE, 2);
I2C_putData(I2CA_BASE, msg->memoryHighAddr);
I2C_putData(I2CA_BASE, msg->memoryLowAddr);
I2C_setConfig(I2CA_BASE, I2C_CONTROLLER_SEND_MODE);
I2C_sendStartCondition(I2CA_BASE);
}
else if(msg->msgStatus == MSG_STATUS_RESTART)
{
//
// Address setup phase has completed. Now setup how many bytes expected
// and send restart as controller-receiver.
//
I2C_setDataCount(I2CA_BASE, (msg->numBytes));
I2C_setConfig(I2CA_BASE, I2C_CONTROLLER_RECEIVE_MODE);
I2C_sendStartCondition(I2CA_BASE);
I2C_sendStopCondition(I2CA_BASE);
}
return(SUCCESS);
}
//
// I2C A ISR (non-FIFO)
//
__interrupt void i2cAISR(void)
{
I2C_InterruptSource intSource;
uint16_t i;
//
// Read interrupt source
//
intSource = I2C_getInterruptSource(I2CA_BASE);
//
// Interrupt source = stop condition detected
//
if(intSource == I2C_INTSRC_STOP_CONDITION)
{
//
// If completed message was writing data, reset msg to inactive state
//
if(currentMsgPtr->msgStatus == MSG_STATUS_WRITE_BUSY)
{
currentMsgPtr->msgStatus = MSG_STATUS_INACTIVE;
}
else
{
//
// If a message receives a NACK during the address setup portion of
// the EEPROM read, the code further below included in the register
// access ready interrupt source code will generate a stop
// condition. After the stop condition is received (here), set the
// message status to try again. User may want to limit the number
// of retries before generating an error.
//
if(currentMsgPtr->msgStatus == MSG_STATUS_SEND_NOSTOP_BUSY)
{
currentMsgPtr->msgStatus = MSG_STATUS_SEND_NOSTOP;
}
//
// If completed message was reading EEPROM data, reset message to
// inactive state and read data from FIFO.
//
else if(currentMsgPtr->msgStatus == MSG_STATUS_READ_BUSY)
{
currentMsgPtr->msgStatus = MSG_STATUS_INACTIVE;
for(i=0; i < NUM_BYTES; i++)
{
currentMsgPtr->msgBuffer[i] = I2C_getData(I2CA_BASE);
}
//
// Check received data
//
for(i=0; i < NUM_BYTES; i++)
{
if(i2cMsgIn.msgBuffer[i] == i2cMsgOut.msgBuffer[i])
{
passCount++;
}
else
{
failCount++;
}
}
if(passCount == NUM_BYTES)
{
pass();
}
else
{
fail();
}
}
}
}
//
// Interrupt source = Register Access Ready
//
// This interrupt is used to determine when the EEPROM address setup
// portion of the read data communication is complete. Since no stop bit
// is commanded, this flag tells us when the message has been sent
// instead of the SCD flag.
//
else if(intSource == I2C_INTSRC_REG_ACCESS_RDY)
{
//
// If a NACK is received, clear the NACK bit and command a stop.
// Otherwise, move on to the read data portion of the communication.
//
if((I2C_getStatus(I2CA_BASE) & I2C_STS_NO_ACK) != 0)
{
I2C_sendStopCondition(I2CA_BASE);
I2C_clearStatus(I2CA_BASE, I2C_STS_NO_ACK);
}
else if(currentMsgPtr->msgStatus == MSG_STATUS_SEND_NOSTOP_BUSY)
{
currentMsgPtr->msgStatus = MSG_STATUS_RESTART;
}
}
else
{
//
// Generate some error from invalid interrupt source
//
asm(" ESTOP0");
}
//
// Issue ACK to enable future group 8 interrupts
//
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP8);
}
//
// Function to be called if data written matches data read
//
void pass(void)
{
asm(" ESTOP0");
for(;;);
}
//
// Function to be called if data written does NOT match data read
//
void fail(void)
{
asm(" ESTOP0");
for(;;);
}