Hello,
I have a problem with the continuous refresh function of the expressions window in CCS 9.2. I knew this is an old version, but I don´t want to change the version during the running project. Yesterday this function has worked properly.
After activating this function the expressions window is only updateted one time and not continuous. After that the expression windows is not updated anymore.
The DSP runs properly, it is possible to click the refresh button and then you will get the actual values. The problem appears with all workspaces I have.
How can I solve this problem?
Thank you
Ralf