This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-HV-1PH-DCAC: CHANGING POWERSUITE PARAMETERS LIKE CUTOFF FREQ.

Part Number: TIDM-HV-1PH-DCAC
Other Parts Discussed in Thread: POWERSUITE, C2000WARE

AM UNABLE TO  EDIT POWERSUITE VALUE

1) Cutoff freq(khz) . I have changed Rfltr to 100ohm, Cfiltr remains 0.22, but cutoff freq remains unchanged.

2. I have similar problem with MaxVbus under Voltage sense and Max current sense(here i changed sensing resistor values and  curent sensor Norminal output voltage)

I checked other reference designs like pfc designs, they are changing fine. where can i change these value so that i can use higher power rating custom design?

check cuffoff freg is unchange in above photo.

AM USING:  CCS 12.6.0

C2000ware_DigitalPower_SDK_5_01_00_00