Part Number: TMS320F28P650DK
Hi Team,
According to the TRM description, some of the GPI or GPO functions of EtherCAT are routed to two pads. The customer tested GPI3. GPI3 is connected to GPIO3 and GPIO103 respectively. But why does this register have no effect on which set of PAD is used, whether it is configured or not?

Regardless of whether this register is configured or not, this function can be used only after configuring the GPIO pinmux. Customers think this is unreasonable.
And could you please explain the general process of using the GPI/GPO function?
--
Thanks & Regards