Part Number: TMS320F2800157
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Dears,
Customer feedback that F2800157SPN below issue,pls kindly help to check it.
1. SPI cannot be configured successfully, and the routine provided by TI (C2000ware) "spi_ex1_loopback" is modified to the SPI main mode on the TI development board, and it is found that the CLK pin has been low and the SIMO pin has been high. Could not actually send data. Please help check, or even better, mention the SPI routine that has been successfully configured.
2, EEPROM debugging also encountered problems, directly transplanted or using routines (C2000ware) can not read and write successfully. Whether there is a relevant success routine provided.
3, 28034 chip program transplant to 2800157 chip whether there are relevant guidance documents
Thanks