This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Program boots when using debugger, but not after power cycle

Part Number: TMS320F28388D
Other Parts Discussed in Thread: SYSCONFIG

Hello,

I've been doing some research and I've seen that other people have this same issue, but I tried everything thas was proposed in other threads and nothing has worked so far.

I'm using the F28388D dev board and SysConfig to configure my project.

I got my CMD file from one of the example projects (2838x_FLASH_CLA_lnk_cpu1.cmd).

The file F2838x_CodeStartBranch.asm has been generated by SysConfig and it has the watchdog disable code that is executed before calling _c_int00.

In project properties > C2000 Linker > Advanced Options > Symbol Management, the entry point is properly defined: code_start.

I've tried flashing several example projects from the "Project Wizard" (like "dual_blinky"), and they work perfectly when I use the debugger, but they don't boot automatically when I power cycle the board.

Thank you in advance for your help!