Other Parts Discussed in Thread: C2000WARE, DRV8353
Working on custom board development and motor is running successfully in custom board .
1)Facing issues in motor running .its oscillates too much .which are the parameters need to consider to reduce oscillation ?
2)Its taking high current and some times initially running in reverse direction after few second started running in forward direction .How to avoid such issues ?
3)is there any way to control motor torque and which are the calibration parameter is required to change motor torque.
4)if motor parameters are updated and make motor_identifications = true, no need to identified again but still expression windows not showing the updated value from user_mtr.h .
every time need to enter the motor parameter values in expression window.which is not updated directly from user_mtr.h
Thanks in Advance
Regards
Shankar Prabhakaran