Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D
Hi Team,
There's an issue from the customer need your help:
Run the ADC in STL's official safety diagnostic library with a resolution of 12, a test program without DMA, enable the DAC-A output, and set the value to 2048. On the LAUNCHXL-F28379D development board by connecting the ADCINA0 pins and ADCINA1 pins, Debug on CCS12, run the program at full speed, observe the value of the ADC result register in the register value window, always on the result that the ADC did not acquire data, suspect that the data sent by the DAC is always 0, not 2048. Tried to acquire using the EPWM and GPIO connected to the ADCINA1 pin of the ADC and the result register has the correct value of the register. What should I do in this situation?
Best Regards,
Ben