Part Number: TMS320F280049
Hi,
We are observing an issue with ADC inputs when reading circuits with high impedance (~5kOhms).
The problem is high leakage into ADC pin which affects the voltage divider. Failure rate is in percent range (~20Pcs out of ~2000Pcs). At least pins C0/19 and A0/23 are affected.
Following circuit shows the ADC circuit. A voltage divider of 10k plus NTC is fed to ADC.

Following scope plot shows on Ch1 = VDDA=VDDIO and Ch2 = C0/pin 19 voltage.
Interestingly at startup the pin voltage is correct (half of 3V, since NTC=10 at 25°C), but after about 1s (can be anything between 0.2 to few seconds), the voltage drops like some breakdown occurs.


More interesting: After turn off supply and restart within few minutes (all voltages are gone), the pin is directly low at startup as shown here:

But after leaving the DSP unpowered for ~15 minutes, the behavior is again as on first scope plot.
ADC reading corresponds always to voltage applied to pin, so ADC itself is seems ok.
Doing this test with DSP reset XRSn kept low results in the same behavior, so FW can be excluded:

Do you see any potential cause that can lead to such a behavior? Can it be some protection circuit that is mistakenly activated?
It seems the parts affected have it from the start. Parts that are ok remain ok also later.
ESD may be excluded, since production is ESD handling compliant.
Any help here would be appreciated.
Best regards,
Urs