Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
hi.
topic: example(C2000Ware_5_01_00_00 )
part: TMS320F28P650DK9ZEJ.
I'm new to TI development and learned about multicore debugging through blog.
I successfully loaded 'empty_sysconfig_256zej' onto CPU1, but 'enet_lwip' doesn't load onto CPU2 or the CLA.
Error: C28xx_CPU2: GEL: File: D:\ti\c2000\C2000Ware_5_01_00_00\libraries\communications\Ethernet\third_party\lwip\examples\enet_lwip\cm\ccs\Flash\enet_lwip_cm.out Does not match the target type, not loaded.
enet_lwip.c is using CM_init() ---> it may require Cortex-M.
However, the TMS320F28P650DK9ZEJ only features CPU1, CLA, and CPU2.
I want to use Ethernet with the TMS320F28P650DK9ZEJ.
I'm not very experienced in development. I need help.