This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28384S: Does the USB support OTG?

Part Number: TMS320F28384S
Other Parts Discussed in Thread: C2000WARE

Dear Champs,

I am asking this for our customer.

Does F2838x USB support OTG?

If not, can the user use another GPIO to mean host or slave and change its USB mode on the fly (during runtime)?

  • Hi, 

    We do not support USB OTG. But we do support both host and device modes. 

    There is an example provided within C2000Ware (usb_ex8_dual_detect) which can be referred . This example uses a GPIO for ID detection and switches between host and device mode .

    Best Regards

    Siddharth