Hello everybody,
I use Embedded Coder for coding F28379D C2000 microcontroller. I generate code for the Launchxl board. I have programed an GPIO to switch from 0 to 1 after 100ms. When I probe this signal with a scope, I can see that during the power-up sequence, the signal rise to 3.3V rapidly and just after goes to 0V and finaly go to 3.3V after 100ms. I want to know, why this signal has this start sequence. Maybe the GPIO are High-Z during power-up ? Is it possible to set an internal pull-down ? How can I do that with Embedded Coder ?
Thank you.
Quentin