This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: configuring interrupts

Part Number: TMS320F280049C

Hi Champ,

I am asking for my customer.

As TRM section 3.5.4.3, it tells the procedures of disabling interrupts. 

It specifies Enable interrupts globally (EINT or CLRC INTM) in step 6 after clearing all the IER/IFR in PIE stage and CPU stage in previous step 2~5. 

(1). Why it is needed to additionally Enable interrupts globally in the end for disabling interrupts ? In my understanding, as soon as the step 2~5 are done, it should disable the peripheral's interrupt request propagating to CPU, correct ? Is the step 6 a must need to do or a suggestion to do ? 

(2). If step 6 isn't done by user for disabling interrupts, what problem would it cause when we try to re-enable interrupts as the procedure specified in section 3.5.4.1 Enabling Interrupts following ? 

Thanks and regards,

Johnny