Part Number: TMS320F28027F
Hello,
I am working on an application where a PC will connect to the LaunchpadXL via serial port. On some boards, there are no issues. The PC will connect to the appropriate COM port, and the application works.
However, on 2 of 4 LaunchpadXL's tested so far, the PC side will not connect to the detected COM port. I see no traffic at the SCI pins on the 28027. The PC side simply provides a "cannot connect" error.
Switch 4 is in the correct position.
I am testing with the LaunchpadXLs powered by USB, with no other hardware connected.
Have you seen similar issues before, or do you have ideas on what the issue may be?
Thanks!