Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: DRV8305, MOTORWARE
I have purchased the F28069M and the DRV8305 to drive a three phase motor, and I have been having a lot of problems. First of all, the quick start guide says that an example program should automatically load when plugged in to a device with all the software(CCS, motorware, control suite) are installed, which did not happen. When we tried the JTAG connection, it only c]became successful when we attached the DRV8305 board to it and supplied it power. Even when the JTAG is successful, when we try to upload any of the example code eg the LED blink code, we get a load program error. We also made sure the target configuration was correct.
.
. Any help with this would be greatly appreciated.