Hi Team,
There's an issue from the customer need your help:


This is the structure of Message RAM, and the yellow highlight of the text explanation next to it says: "There is no restriction on the order of the segments".
Can I understand that when I use it, as long as it does not exceed the limit of 2048 words, any segment in RAM, for example
The Rx FIFO0 part can be placed either in the position of the 11-bit Filter shown in the diagram or in the position of the Tx Buffers. And at the same time
The 11-bit filter can also be placed behind the Rx FIFO0.
Best Regards,
Ben