Part Number: TMS320F28335
The TMS320F28335 file downloaded from the Internet cannot be imported.
According to the download description: CCS6.0 environment, based on DSP28335 brushless DC motor control program code with Hall sensor, including all files such as header file and main program. The speed closed-loop control is applied in the main program.
I tested with CCS10.0 and ccs6.1 respectively, and neither of them could be imported normally.
How should we solve this problem?