Hello experts,
I read the technical document SFFS022
I noticed that only the 1oo1D security architecture is mentioned in relation to the dual-core microcontroller TMS320F2838xD. I'm wondering if a 1oo2 security architecture is feasible with this dual-core microcontroller or not.
I imagine the following application. A motor with 2 encoders is powered by a power amplifier with TMS320F2838xD.
The first channel: The motor control and motion function are implemented on the first core (CPU + CLA). This core uses the positions from the first encoder.
The second channel: The second core (CPU + CLA) reads the second encoder to monitor the motor position.
By comparing the positions from these two channels, it is possible to implement not only STO (Safe Torque Off) but also SS1 (Safe Stop 1), SOS (Safe Operating Stop), SLS (Safe Limiting Speed) or SDI (Safe Direction). All of these operating modes already require safety architecture 1oo2. This means that SIL3 is also possible.
Am I right with my train of thought here or am I making a mistake somewhere?
Many thanks in advance and best regards
Bui