Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Hello,
I am using this DSP for my project. I am using ePWM to control inverter legs, and DC/DC.
I have set the PWMs with Active Low Complementary with deadband. I have issue that when DSP is initializing and for a short while, both the PWM pins get active.
To make sure I have not done any thing wrong, I tested your original example code from C2000Ware_4_03_00_00. It is still the same. At start up and for a short while, both PWMs are low (active).
This causes shoot through in my inverter, failing all the MOSFETs.
I have used the "epwm_ex8_deadband" of the following example folder:
C:\ti\c2000\C2000Ware_4_03_00_00\driverlib\f2838x\examples\c28x\epwm
I am attaching you the waveforms I captured at start up. I attached two pull ups to the ePWM5 (active low complementary) pins to properly differentiate between high, and high z states.
Then, I set the trigger to dropping edge, single shot.
I appreciate your help,
Thanks,
Ali