Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hello everyone,
We are trying to boot (programing) via USB option but it is not working.
Steps:
- Connecting the target with SW: 1 1 and ASW1: 1 1
- Opening memory browser and updating memory location 0xD00 with 0x0C5A
- After second step, we connect USB from Micro USB Port on top of TMS320F28379D Control Card to PC.
- Then resetting CPU via CSS (Fig-1)
- Pressing run button on CSS.

Fig-1. CPU Reset Command

Fig-2. Memory Browser

Fig-3. Unknown USB Device in Device Manager
This output is only seen with F2837xD_usb_flash_kernels_cpu01. When we attemped the simple LED blink example for USB boot, the 'Unknown USB Device' does not appear as shown in Fig-3.
You can see Unknown USB Device Information as follows;
Device USB\VID_0000&PID_0002\6&8bfbd&0&4 was configured.
Driver Name: usb.inf
Class Guid: {36fc9e60-c465-11cf-8056-444553540000}
Driver Date: 06/21/2006
Driver Version: 10.0.19041.4046
Driver Provider: Microsoft
Driver Section: BADDEVICE.Dev.NT
Driver Rank: 0xFF0000
Matching Device Id: USB\DEVICE_DESCRIPTOR_FAILURE
Outranked Drivers: usb.inf:USB\DEVICE_DESCRIPTOR_FAILURE:00FF2000
Device Updated: false
Parent Device: USB\VID_05E3&PID_0610\5&2eda7e1e&0&1
Best Regards,
Furkan S.