Part Number: TMDSCNCD28035ISO
Hello,
For a project I want to test a string of 0.5V solar cells. I am attaching the link of the cells that I would be using. Since I would be using only 10 such cells the input voltage would only be around 5V. Using a DC flyback converter I am expecting a DC voltage bus of around 15V output. I wanted to know if the TMDSSOLARUINVKIT works for such a setup. I am new to firmware development and want to use the kit's firmware to implement the MPPT and all the ISRs as depicted in the kit's documents.
www.amazon.com/.../B081Y6R85N