Part Number: TMS320F280049C-Q1
Hello ,
Could you please provide feedback for the below queries:
1. If the orderable part number or MPN F280049CPZQR is a automotive qualified part.
If not please let know the orderable part number.
2. Is monitoring VDDIO suggested since it has internal Monitoring?
In our use case we are using Internal LDO/DC DC for VDD. So in this case do you suggest monitoring the power rails?
3. Regarding crystal , I see a suggestion of 6 to 12pF load capacitance in datasheet but in the EVM it uses 18pF part , can we go ahead with the same?
https://www.ti.com/lit/zip/sprr421 - This is the EVM referred.
4. Do you have a tool which calculates the overall power dissipation / calculation based on the peripherals which are used?
I see only one current info given with specified use case. We are using GPIOs from uC which needs to drive external signals , so how to calculate the power dissipation in this case.
Thank you in advance!