Part Number: TMS320F28234
Hi,
I am using ccs version 8.3.1 and emulator XDS510 usb for a custom board with F28234. The setup was working fine previously but now it is showing emulator rest error and when test connection in target configuration is checked following error is showing.
Execute the command:
%ccs_base%/emulation/drivers/sdjtag.exe -f %boarddatafile% -v -X reset -X scantest
[Result]
** BoardFilePath: C:\Users\PEG145D\AppData\Local\TEXASI~1\CCS\ti\0\0\BrdDat\testBoard.dat
** Resetting Emulator
ERROR -- XDS510USB Reset Failed
ERROR -- Check power to your emulator/eZdsp
ERROR -- Then check your port address
[End: Spectrum Digital XDS510USB Emulator_0]
I tried different Emulator but same issue. I have tried SDconfigX but showing same error. Checked JTAG voltage levels which is ok. What may be the issue?
Regards,
Nandu