Hello, Team,
First, I’ d like to show my gratitude towards the team who supported me to consider prototyping the converter kindly last year.
I’d like to ask about the target customer and the estimated applications of the converter.
As you know, nowadays, various types of bi-directional DC-DC converter are developed all over the globe. Especially, I often see some converters whose nominal low voltage outputs are 48V are released. However, I’ve hardly seen the converters whose nominal low voltage outputs are 12V, like TIDM-BIDIR-400-12.
I assume that this is attributed to the needs in the world or something. Also, according to the design guide, I assume that the reason why the nominal low voltage output of the converter is 12V is to charge the battery.
Based on the above expectations, I’d like to ask you the target customer and the estimated applications of the converter, in other words, the purpose of developing the converter in detail.
Also, if you know, I’d like to ask the reason why the converters whose nominal low voltage outputs are 48V are mainly released.
I appreciate your every support.
Best Regards,
Takumi