Part Number: TMS320F28386S
Other Parts Discussed in Thread: TMDSCNCD28388D, C2000WARE
Hello Team,
I'm working with a customer to interleave 2 or 4 ADC within the F2838xS, using the TMDSCNCD28388D.
On the P650 interleaving would work ok since there is a delay option to trigger the ADC via the timer.
For the F2838xSI want to ask if something similar to the MSPM0 would be possibile.
for two ADC:
I want to achieve same sampling time between samples, which are taken by two ADC, working in interleaving mode (same input).
On the MSPM0, I can use a timer, with two compare units, and each compare unit is set to make a PWM signal, at same frequency and complementary output to the other compare unit.
The output signal of each compare unit triggers one ADC. In this way I can trigger two ADCs with the same frequency, but out of phase.
The result is that distance of each sample is the same, and the result sampling frequency of the two ADC together is twice the single ADC.
- Can the C2000 timer and two compare units trigger two different ADC (one per compare unit)?
- Can I do it with 4?
The problem of using different timers, is that I may not be able to get exact sampling period, due to the configuration overload and different start time.
Thanks,
Mauro