Other Parts Discussed in Thread: C2000WARE
Hi,
So i am trying to implement CLA_FFT on MCU F28069M but am unable to execute it.
firstly Can this MCU run a 1024 point FFT.
Trying to Execute below Functions:
__interrupt void
Cla1Task1 (void)
{
__mdebugstop();
CLA_CFFT_run1024Pt();
__mdebugstop();
CLA_CFFT_unpack512Pt();
}Also here is the linker command file i have designed to execute FFT and FIR through CLA
_Cla1Prog_Start = _Cla1funcsRunStart;
-heap 0x400
-stack 0x400
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
// CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
RAMM0M1 : origin = 0x000050, length = 0x000750
RAML5 : origin = 0x00E000, length = 0x002000
FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */
FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */
ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
/* RAML0_L2 : origin = 0x008000, length = 0x001000 */
RAML3 : origin = 0x009000, length = 0x001000
/* FPU Tables in Boot ROM */
FPUTABLES : origin = 0x3FD590, length = 0x0006A0
/* IQ Math Tables in Boot ROM */
IQTABLES : origin = 0x3FDF00, length = 0x000B50
IQTABLES2 : origin = 0x3FEA50, length = 0x00008C
IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA
PAGE 1 :
CLARAM0 : origin = 0x008800, length = 0x000400
CLARAM1 : origin = 0x008C00, length = 0x000400
CLARAM2 : origin = 0x008000, length = 0x000800
/* on-chip RAM block L4-L8 */
RAML4 : origin = 0x00A000, length = 0x04000
RAML5_2 : origin = 0x010000, length = 0x001000
RAML6 : origin = 0x011000, length = 0x001000
RAML7 : origin = 0x012000, length = 0x001000
RAML8 : origin = 0x013000, length = 0x001000
USB_RAM : origin = 0x040000, length = 0x000800 /* USB RAM */
FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
}
SECTIONS
{
/* Setup for "boot to SARAM" mode:
The codestart section (found in DSP28_CodeStartBranch.asm)
re-directs execution to the start of user code. */
ramfuncs : LOAD = FLASHD,
RUN = RAML5,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
LOAD_SIZE(_RamfuncsLoadSize),
PAGE = 0
.cinit : > FLASHA, PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA, PAGE = 0
codestart : > BEGIN, PAGE = 0
/* Allocate uninitialized data sections: */
.stack : > RAMM0M1, PAGE = 0
.ebss : > RAML4, PAGE = 1
.esysmem : > RAML4, PAGE = 1
.cio : > RAML4, PAGE = 1
/* Initialized sections to go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA, PAGE = 0
.switch : > FLASHA, PAGE = 0
.scratchpad : > CLARAM0, PAGE = 1
.bss_cla : > CLARAM0, PAGE = 1
.const_cla : > CLARAM0, PAGE = 1
IQmath : > FLASHB, PAGE = 1
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
// CLA1fftTables : > RAML3, PAGE = 1
/* Allocate FPU math areas: */
FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD
RFFTdata1 : > RAML6, PAGE = 1
RFFTdata2 : > RAML7, PAGE = 1
RFFTdata3 : > RAML8, PAGE = 1
RFFTdata4 : > RAML5_2, PAGE = 1
Cla1Prog : > RAML3,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
LOAD_SIZE(_Cla1funcsLoadSize),
RUN_START(_Cla1funcsRunStart),
PAGE = 0
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
Cla1DataRam0 : > CLARAM0, PAGE = 1
Cla1DataRam1 : > CLARAM1, PAGE = 1
Cla1DataRam2 : > CLARAM2, PAGE = 1
CLA1mathTables : > CLARAM1,
LOAD_START(_Cla1mathTablesLoadStart),
LOAD_END(_Cla1mathTablesLoadEnd),
LOAD_SIZE(_Cla1mathTablesLoadSize),
RUN_START(_Cla1mathTablesRunStart),
PAGE = 1
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > CLARAM0,
PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS, PAGE = 0, TYPE = DSECTI am unable to find any Example code for implementing FFT on this MCU.
Kindly guide me whether it is acheivable or not.
Also please help identify the fault in above and how should i go about it.
I am measuring vibration of a engine using a ADXL359 accelerometer sensor.
As I am Sampling data at every 1 millisecond, i am using FFT 1024 point for higher accuracy.
But its taking a lot more time in computation