This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280049C: 3V reference for ADC

Part Number: LAUNCHXL-F280049C

we can give 3V reference for ADC  but in API We have 3.3V and 2.5V  for 3V ADC reference what i should do ?

  • Hello Subash,

    3V is not an option for the ADC reference, there is internal 2.5 or 3.3 or external 3.3. Technically it is possible to use an external 3V reference by lowering the supply voltage to 3V (see the Recommended Operating Conditions and ADC Operating Conditions tables in the datasheet), but you would need to make sure that VDDA (analog supply voltage) never dips below the minimum stated in the datasheet. This is up to you if you want to do this or use an internal reference instead if you can't change from an external reference of 3V.

  • i will check 3V with external Reference