Part Number: TMS320F28379S
Hi Champ,
I am asking for my customer.
They are designing their own daughter card with F28379S, then insert the daughter card into their PSU.
Since we will debug the device via in CCS debug mode in the beginning, and once finished the all peripherals validation, they will finally run the device in standalone mode with flash boot in PSU, and only connect JTAG for re-programming the fw code, rarely need debug via JTAG in CCS debug mode anymore.
So, in the beginning for the hw design, we should have them to put a switch or externally reserve a pull high/low circuit on TRST pin in advance, to switch the TRST pin status from 1 to 0, correct ?
Thanks and regards,
Johnny