Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, CODECOMPOSER
I wrote a custom bootloader that stores an application in flash.
When I run the bootloader, its initialization completes successfully, it then detects the application resides in flash and starts the application at a specific address.
By using the debugger and "Assembly Step Into"/"Assembly Step Over" (because I don't have the application's symbols loaded, only the bootloader is loaded in the debugger), I found that the application hangs inside InitSysPll(), specifically when waiting for the SYSPLL lock counter (sysctl.c:363):
//
// Lock the PLL five times. This helps ensure a successful start.
// Five is the minimum recommended number. The user can increase
// this number according to allotted system initialization time.
//
for(i = 0U; i < 5U; i++)
{
//
// Turn off PLL
//
HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLCTL1) &=
~SYSCTL_SYSPLLCTL1_PLLEN;
asm(" RPT #60 || NOP");
//
// Write multiplier, which automatically turns on the PLL
//
HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLMULT) = pllMult;
//
// Wait for the SYSPLL lock counter
//
while((HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLSTS) &
SYSCTL_SYSPLLSTS_LOCKS) == 0U)
{
//
// Consider to servicing the watchdog using
// SysCtl_serviceWatchdog()
//
}
}
Both the bootloader and the application call F2837xD_SysCtrl.c's InitSysCtrl().
If I debug the application (without the bootloader), its initialization works fine, it doesn't hang inside InitSysCtrl().
Do I have to do something in the bootloader to unlock the SYSPLL before starting the application?
Thank you,
Diane