Hello everyone,
Recently I am using CMPSS for AC current CBC protection, its negative input is a fixed threshold of 80A, and the positive input is ADC sampling, and I found that sometimes the current exceeds 80A in a short period of time will not trigger the protection of CMPSS, so I want to know if the output of CMPSS is limited by the sampling rate of ADC?
I still have a doubt about the sampling rate of the ADC, that is, the ADC port is a real-time value, is the data captured as the system clock, and the conversion will be maintained after the trigger source appears?