Part Number: TMS320F28P650SH
Hi Champs,
Customer now is designing the schematic diagram and PCB. They found that there were many via holes at the bottom of the 176pin package. Customer want to know whether all four layers of copper must be laid at the bottom of the DSP? Or can the board's surface layer of DSP part not be laid with copper? Because customer are worried that if the surface layer is also covered with copper, there will be overflowing solder connected to the pins.
Do we have any requirements for the copper laying of circuit boards? Customer wants to know if there is no copper on the surface under the DSP. Thanks!

Best Regards,
Julia