Can I run the processor at 120MHz instead of 60MHz? What about 240MHz? What about 1.2Ghz? What is the limitation on speed with these devices?
My situation is I am using a TMS320F28035 to operate a dc/dc converter. Unfortunately, at the frequency at which I would like to operate (500KHz), my CMPx register is only 120 counts (ePWM Clock = 60MHz), and this doesn't give very good output resolution when the input is 100V. Is there another way to get more resolution from the ePWM modules?