Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE, TIDM-1000, POWERSUITE, SYSCONFIG
Dear TI experts,
I am reaching out to seek clarification on a couple of issues I encountered with the Syscfg tool in the C2000Ware_DigitalPower exemplary project, post-installation (as shown below).

(1) I noticed a setting labeled "INCR_BUILD" in the Syscfg tool. I assumed changes to this setting would reflect in the "VIENNA_INCR_BUILD" value in the code snippet. However, altering the "INCR_BUILD" value seems to have no effect on the corresponding code. Could you provide guidance on how this setting is supposed to interact with the code?


(2) Additionally, the Syscfg tool typically auto-generates "board.c" or "board.h" files in many exemplary projects within C2000Ware. In this instance, I was unable to locate these files. Does Syscfg create a different set of files in this context, or how should the absence of these usual files affect the code structure?

Thanks,
Eric